TJA1100 Rx and Tx Failure Count

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1100 Rx and Tx Failure Count

1,856件の閲覧回数
shanmugamsundar
Contributor IV

Hi,

We are using TJA1100 for our automotive applications. We have requirement to send out the PHY Rx and Tx failure count.

In Datasheet I can find the register address 26 (Link fail counter register).Which is counting Local receiver error count and Remote receiver error count.

We cannot understand completely the Local and remote receiver error counts. And How it related with Tx and Rx failure counts.

For example:

Can we assume like below

   Local receiver count = Tx failure

   Remote receiver count = Rx Failure

Can someone clarify the above doubts.

Thanks,

Shan

ラベル(1)
0 件の賞賛
返信
1 返信

1,574件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You can refer to

TJA1100 pin4&16 ; C26 & C28 

TJA1100 in imx6 with Managed mode 

https://community.nxp.com/message/925234 

Hope these can do help for you.

Have a nice day

Rita

0 件の賞賛
返信