TEMPMON accuracy without RTC XTAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEMPMON accuracy without RTC XTAL

Jump to solution
1,840 Views
fredstewart
Contributor I

We intend to use the i.MX6 Dual without the RTC crystal, yet I see that TEMPMON takes the 32KHz clock as input. Will the ring oscillator wide frequency tolerance lead to inaccurate die temperature readings?

Labels (3)
0 Kudos
Reply
1 Solution
1,661 Views
igorpadykov
NXP Employee
NXP Employee

Hi fred

no ring oscillator will not introduce additional inaccuracies.

BTW operation without crystal is not recommended due to ERR007926.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,662 Views
igorpadykov
NXP Employee
NXP Employee

Hi fred

no ring oscillator will not introduce additional inaccuracies.

BTW operation without crystal is not recommended due to ERR007926.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply