TEMPMON accuracy without RTC XTAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEMPMON accuracy without RTC XTAL

ソリューションへジャンプ
1,875件の閲覧回数
fredstewart
Contributor I

We intend to use the i.MX6 Dual without the RTC crystal, yet I see that TEMPMON takes the 32KHz clock as input. Will the ring oscillator wide frequency tolerance lead to inaccurate die temperature readings?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,696件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fred

no ring oscillator will not introduce additional inaccuracies.

BTW operation without crystal is not recommended due to ERR007926.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,697件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fred

no ring oscillator will not introduce additional inaccuracies.

BTW operation without crystal is not recommended due to ERR007926.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信