TAMPER DETECTION: WHICH PINS & WHICH REGISTER?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TAMPER DETECTION: WHICH PINS & WHICH REGISTER?

1,526 Views
imme_jakobeit
Contributor I

Project: Connect a wire onto the tamper Pins of the iMX6ULL-EVK Board and if you cut it, the board will detect it and                     delete the security keys.

Problem: Do I connect the wire to a SNVS_TAMPER Pin and GND? 

               If thats possible, what Registers do I have to set in order to delete the keys?

Thanks for the help.

Labels (1)
Tags (1)
1 Reply

1,345 Views
igorpadykov
NXP Employee
NXP Employee

Hi Imme

please check answer on

https://community.nxp.com/message/1027146?commentID=1027146#comment-1027146 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply