HOW TO TEST CAN PROTOCOL IN IMX6ULEVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HOW TO TEST CAN PROTOCOL IN IMX6ULEVK

1,383 Views
nagaprasadvasam
Contributor III

Hi Everyone,

                  I need to test can protocol on imx6ul evk,i have tried to test can using can-utils but it is not working properly,can anyone please help me how i need to enable communication  using   imx board and externally connected Board.

Thanks & Regards,

Prasad.

0 Kudos
Reply
1 Reply

1,284 Views
igorpadykov
NXP Employee
NXP Employee

Hi nagaprasad

one can test with unit tests (imx-test, ..test/can  folder)

imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

use Demo Image

i.MX 6UltraLite EVK Linux Binary Demo Files

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_iMX6UL&appType=license&location=null&Paren... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply