System be hanged after reboot command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System be hanged after reboot command

3,232 Views
wangvictor
Contributor III

Hi Community,

I'm working on i.MX6 sabreSD DL and using linux kernel L4.1.15.

My hardware designed will connect WDOG_B to PMIC Control PWRON.

After I send reboot command WDOG_B will reset and cause PMIC Control PWRON reset too.

Then the system be hanged like below log.

root@arm:~# reboot
[ OK ] Stopped target Timers.
Stopping User Manager for UID 0...
Stopping Authorization Manager...
Starting Unattended Upgrades...
Stopping Session c1 of user hermes.
Stopping User Manager for UID 1001...
[ OK ] Stopped Daily Cleanup of Temporary Directories.
Stopping Disk Manager...
[ OK ] Stopped target Graphical Interface.
Stopping Light Display Manager...
[ OK ] Stopped target Multi-User System.
Stopping OpenBSD Secure Shell server...
Stopping Avahi mDNS/DNS-SD Stack...
Stopping LSB: Apache2 web server...
Stopping Modem Manager...
Stopping LSB: set CPUFreq kernel parameters...
Stopping LSB: Start busybox udhcpd at boot time...
Stopping LSB: Advanced IEEE 802.11 management daemon...
Stopping D-Bus System Message Bus...
Stopping Regular background program processing daemon...
Stopping Stopping Session c2 of user root.
Stopping LSB: Starts and stops Wicd...
[ OK ] Stopped target Login Prompts.
Stopping Serial Getty on ttymxc0...
Stopping Getty on tty1...
[ OK ] Stopped Modem Manager.
[ OK ] Stopped Avahi mDNS/DNS-SD Stack.
[ OK ] Stopped OpenBSD Secure Shell server.
[ OK ] Stopped Regular background program processing daemon.
[ OK ] Stopped System Logging Service.
[ 1961.034311] imx-ipuv3 2400000.ipu: WARNING: adapt panel end blank lines
[ OK ] Stopped D-Bus System Message Bus.
[ 1961.176691] imx-ipuv3 2400000.ipu: WARNING: adapt panel end blank lines
[ OK ] Stopped Authorization Manager.
[ OK ] Stopped Serial Getty on ttymxc0.
[ OK ] Stopped Getty on tty1.
[ OK ] Stopped Light Display Manager.
[ OK ] Stopped User Manager for UID 1001.
[ OK ] Stopped Disk Manager.
[ OK ] Stopped User Manager for UID 0.
[ OK ] Stopped Session c1 of user hermes.
[ OK ] Stopped LSB: Advanced IEEE 802.11 management daemon.
[ OK ] Started Unattended Upgrades.
[ OK ] Stopped Session c2 of user root.
[ OK ] Stopped LSB: Start busybox udhcpd at boot time.
[ OK ] Stopped LSB: set CPUFreq kernel parameters.
Stopping LSB: Load kernel modules needed to enable cpufreq scaling...
[ OK ] Removed slice User Slice of root.
[ OK ] Removed slice User Slice of hermes.
Stopping Login Service...
[ OK ] Removed slice system-getty.slice.
Stopping Permit User Sessions...
[ OK ] Removed slice system-serial\x2dgetty.slice.
[ OK ] Stopped /etc/rc.local Compatibility.
[ OK ] Stopped Login Service.
[ OK ] Stopped LSB: Starts and stops Wicd.
[ OK ] Stopped Permit User Sessions.
[ OK ] Stopped LSB: Load kernel modules needed to enable cpufreq scaling.
[ OK ] Stopped LSB: Apache2 web server.
[ OK ] Stopped target Basic System.
[ OK ] Stopped target Paths.
[ OK ] Stopped Dispatch Password Requests to Console Directory Watch.
[ OK ] Stopped Forward Password Requests to Wall Directory Watch.
[ OK ] Stopped target Sockets.
[ OK ] Closed Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Closed D-Bus System Message Bus Socket.
[ OK ] Closed Syslog Socket.
[ OK ] Stopped target Slices.
[ OK ] Removed slice User and Session Slice.
[ OK ] Stopped target Remote File Systems.
[ OK ] Stopped target Remote File Systems (Pre).
[ OK ] Stopped target System Initialization.
[ OK ] Stopped target Encrypted Volumes.
Stopping LSB: NFS support files common to client and server...
Stopping Load/Save Random Seed...
[ OK ] Stopped target Swap.
[ OK ] Stopped Load/Save Random Seed.
[ OK ] Unmounted /run/rpc_pipefs.
[ OK ] Stopped LSB: NFS support files common to client and server.
[ OK ] Stopped target System Time Synchronized.
Stopping Network Time Synchronization...
[ OK ] Stopped target RPC Port Mapper.
Stopping LSB: RPC portmapper replacement...
[ OK ] Stopped Network Time Synchronization.
[ OK ] Stopped Create Volatile Files and Directories.
[ OK ] Stopped LSB: RPC portmapper replacement.
[ OK ] Stopped target Network is Online.
[ OK ] Stopped target Network.
Stopping Raise network interfaces...
[ OK ] Stopped Raise network interfaces.
[ OK ] Stopped Apply Kernel Variables.
[ OK ] Stopped target Local File Systems.
Unmounting /run/user/0...
Unmounting /run/user/1001...
Unmounting /media/hermes/002D-F50C...
[ OK ] Unmounted /run/user/0.
[ OK ] Unmounted /run/user/1001.
[ OK ] Unmounted /media/hermes/002D-F50C.
[ OK ] Reached target Unmount All Filesystems.
[ OK ] Stopped target Local File Systems (Pre).
[ OK ] Stopped Create Static Device Nodes in /dev.
[ OK ] Stopped Remount Root and Kernel File Systems.
[ OK ] Reached target Shutdown.
[ 1966.916231] systemd-shutdown[1]: Sending SIGTERM to remaining processes...
[ 1966.939626] systemd-journald[183]: Received SIGTERM from PID 1 (systemd-shutdow).
[ 1966.984871] systemd-shutdown[1]: Sending SIGKILL to remaining processes...
[ 1967.006239] systemd-shutdown[1]: Hardware watchdog 'imx2+ watchdog', version 0
[ 1967.014752] systemd-shutdown[1]: Unmounting file systems.
[ 1967.020687] systemd-shutdown[1]: Remounting '/' read-only with options 'data=ordered'.
[ 1967.115775] EXT4-fs (mmcblk3p2): re-mounted. Opts: data=ordered
[ 1967.147271] systemd-shutdown[1]: Remounting '/' read-only with options 'data=ordered'.
[ 1967.155680] EXT4-fs (mmcblk3p2): re-mounted. Opts: data=ordered
[ 1967.161727] systemd-shutdown[1]: All filesystems unmounted.
[ 1967.167423] systemd-shutdown[1]: Deactivating swaps.
[ 1967.172784] systemd-shutdown[1]: All swaps deactivated.
[ 1967.178408] systemd-shutdown[1]: Detaching loop devices.
[ 1967.203526] systemd-shutdown[1]: All loop devices detached.
[ 1967.209509] systemd-shutdown[1]: Detaching DM devices.
[ 1967.215642] systemd-shutdown[1]: All DM devices detached.
[ 1967.228790] systemd-shutdown[1]: Failed to read reboot parameter file: No such file or directory
[ 1967.237662] systemd-shutdown[1]: Rebooting.
[ 1967.241858] reboot: winmate victor LINUX_REBOOT_CMD_RESTART
[ 1968.255339] sd 0:0:0:0: [sda] Synchronizing SCSI cache
[ 1968.261816] imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
[ 1968.268248] PM: winmate victor PMIC not shutdown
[ 1968.272891] PM: winmate victor PMIC not shutdown
[ 1968.277560] PM: winmate victor PMIC not shutdown
[ 1968.282198] PM: winmate victor PMIC not shutdown
[ 1968.286861] PM: winmate victor PMIC not shutdown
[ 1968.291496] PM: winmate victor PMIC not shutdown
[ 1968.296160] PM: winmate victor PMIC not shutdown
[ 1968.300795] reboot: winmate victor Restarting system
[ 1968.305813] winmate victor do kernel restart

Before I do reboot command I saw that uboot setting showed Reset cause: POR

U-Boot 2015.04imx_v2015.04_4.1.15_1.2.0_ga+ge1eae17 (Mar 15 2017 - 19:44:21)

CPU: Freescale i.MX6DL rev1.3 at 792 MHz
CPU: Temperature 43 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 2 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

I tried to measure three signals of PMIC Control like below.

  1. STANDBY
  2.  PWRON(connect to WDOG_B )
  3. SW2(gen33 which is EMMC power)

999.jpg

Assuming that main reason why system cannot restart after reboot is because when WDOG_B reset then pwron reset too.

And when pwron reset will cause standby signal high then SW2 will be low-high once.

Because of this cpu cannot recognize Emmc so the machine be handed like picture above.

Is anything I missed and how can I fix this problem?

0 Kudos
Reply
1 Reply

2,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi victor

reason may be both hardware and software, so for narrow downing issue one

can try to reproduce issue on NXP Sabre SD reference board and try with

Demo Images from link

i.MX Software|NXP 

Also if there is no attached coincell to pmic licell, one can try with coincell.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply