PMIC ERROR ON U-BOOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC ERROR ON U-BOOT

1,572 Views
pavandornadula7
Contributor I

U-Boot 2017.03 (Aug 02 2018 - 15:48:56 +0530)

CPU: Freescale i.MX6DP rev1.0 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 32C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
ERROR: read error from device: 4ef40860 register: 0x0!
at drivers/power/pmic/pfuze100.c:46/pfuze100_read()
ERROR: read error from device: 4ef40860 register: 0x3!
at drivers/power/pmic/pfuze100.c:46/pfuze100_read()
PMIC: PFUZE100! DEV_ID=0xfffffffb REV_ID=0xfffffffb
ERROR: read error from device: 4ef40860 register: 0x21!
at drivers/power/pmic/pfuze100.c:46/pfuze100_read()
ERROR: write error to device: 4ef40860 register: 0x21!
at drivers/power/pmic/pfuze100.c:36/pfuze100_write()
ERROR: read error from device: 4ef40860 register: 0x24!
at drivers/power/pmic/pfuze100.c:46/pfuze100_read()
ERROR: write error to device: 4ef40860 register: 0x24!
at drivers/power/pmic/pfuze100.c:36/pfuze100_write()
ERROR: read error from device: 4ef40860 register: 0x2f!
at drivers/power/pmic/pfuze100.c:46/pfuze100_read()
ERROR: write error to device: 4ef40860 register: 0x2f!
at drivers/power/pmic/pfuze100.c:36/pfuze100_write()
ERROR: read error from device: 4ef40860 register: 0x32!
at drivers/power/pmic/pfuze100.c:46/pfuze100_read()
ERROR: write error to device: 4ef40860 register: 0x32!
at drivers/power/pmic/pfuze100.c:36/pfuze100_write()
ERROR: read error from device: 4ef40860 register: 0x0!
at drivers/power/pmic/pfuze100.c:46/pfuze100_read()
Not supported, id=11
initcall sequence 4ffa853c failed at call 17804790 (err=-22)
### ERROR ### Please RESET the board ###

0 Kudos
Reply
3 Replies

1,242 Views
igorpadykov
NXP Employee
NXP Employee

Hi pavan

one can check hardware and i2c signals with oscilloscope, using example connections in

Schematics (3)
Design files, including hardware schematics, Gerbers, and OrCAD files
for i.MX 6QuadPlus (i.MX 6DualPlus emulation)

i.MX 6QuadPlus SABRE Development Board|NXP 

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,243 Views
pavandornadula7
Contributor I

Hi ,

I am checking my board_defconfig file  and i need to be disable any thing like :

CONFIG_DM_PFUZE=Y :----> I NEED TO ENABLE OR DISABLE THIS OPTION 

---> IF YES WHY NEED TO DISABLE 

rEGARDS

PAVAN

0 Kudos
Reply

1,243 Views
igorpadykov
NXP Employee
NXP Employee

Hi pavan

nxp bsps do not have configurations without pmic

Best regards
igor

0 Kudos
Reply