Aline,
I have discovered that libfslxec, as found in several online git repos, derives from imx.5 reference hardware and requires the use of libipu.so.
| 0x00000001 (NEEDED) | Shared library: [libutils.so] |
| 0x00000001 (NEEDED) | Shared library: [libc.so] |
| 0x00000001 (NEEDED) | Shared library: [liblog.so] |
| 0x00000001 (NEEDED) | Shared library: [libcutils.so] |
| 0x00000001 (NEEDED) | Shared library: [libipu.so] |
| 0x00000001 (NEEDED) | Shared library: [libstdc++.so] |
| 0x00000001 (NEEDED) | Shared library: [libm.so] |
libipu is available in the Android imx.6 BSP (at least it's in mine), but the make file has define statements around it to only build if the board has an IPU and it is an imx.5 based device. Therefore, based on this piece of information and the thread at imx6 lib ipu I am left to conclude that you either update the OMXplayer to work with /dev/mxc_ipu or you just live with this error message.
Michael Robbeloth