Hi,
We are thinking of customized IMX6D board with single channel 16-bit
LPDDR2 and would like to know whether IMX6D will support single channel
16-bit LPDDR2. If So, If we connect only 16-bit single channel LPDDR2,
whether the board works fine or we need to connect 4 nos of single channel
LPDDR-2.
If Single channel 16-bit LPDDR2 is not supported then whether Single
channel 32-bit LPDDR2 will be sufficient for our design or we should go for
2x32-bit LPDDR2.