Support of Camera module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Support of Camera module

跳至解决方案
1,002 次查看
nav09
Contributor II

Hello, 

For our application, we have choosed IMX8M-plus processor and the camera sensor from the omnivision (OSO2H10), 

we are interested to know,

  1. If IMX8M-plus supports the firmware for OSO2H10 camera sensor?
  2. OSO2H10 is a raw sensor without any ISP, we have chosen IMX8M-plus to use the ISP within the processor, do you support the tunning of ISP for this camera module?
  3. Kindly share the list of camera modules/sensor supported for IMX8M-plus.

Thanks, 

0 项奖励
回复
1 解答
954 次查看
nav09
Contributor II

Thanks for the response and the links!

Understood, using the reference of OV5640, I can develop the driver for OSO2H10.

I can use available API for ISP tunning.

Regards,

在原帖中查看解决方案

0 项奖励
回复
2 回复数
955 次查看
nav09
Contributor II

Thanks for the response and the links!

Understood, using the reference of OV5640, I can develop the driver for OSO2H10.

I can use available API for ISP tunning.

Regards,

0 项奖励
回复
977 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The OSO2H10 is not support be default on MX8Mplus but it support the OV5640 and should be similar the driver for it you can migrate to your camera with the ISP usage please check:

 

https://www.nxp.com/docs/en/user-guide/iMX8MP_CAMERA_DISPLAY_GUIDE.pdf

https://www.mouser.com/datasheet/2/302/AN13736-3073771.pdf?srsltid=AfmBOoobASIHe4SOtrDvchLUQZebrqyxV...

 

Regards

0 项奖励
回复