Support of Camera module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support of Camera module

Jump to solution
1,006 Views
nav09
Contributor II

Hello, 

For our application, we have choosed IMX8M-plus processor and the camera sensor from the omnivision (OSO2H10), 

we are interested to know,

  1. If IMX8M-plus supports the firmware for OSO2H10 camera sensor?
  2. OSO2H10 is a raw sensor without any ISP, we have chosen IMX8M-plus to use the ISP within the processor, do you support the tunning of ISP for this camera module?
  3. Kindly share the list of camera modules/sensor supported for IMX8M-plus.

Thanks, 

0 Kudos
Reply
1 Solution
958 Views
nav09
Contributor II

Thanks for the response and the links!

Understood, using the reference of OV5640, I can develop the driver for OSO2H10.

I can use available API for ISP tunning.

Regards,

View solution in original post

0 Kudos
Reply
2 Replies
959 Views
nav09
Contributor II

Thanks for the response and the links!

Understood, using the reference of OV5640, I can develop the driver for OSO2H10.

I can use available API for ISP tunning.

Regards,

0 Kudos
Reply
981 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The OSO2H10 is not support be default on MX8Mplus but it support the OV5640 and should be similar the driver for it you can migrate to your camera with the ISP usage please check:

 

https://www.nxp.com/docs/en/user-guide/iMX8MP_CAMERA_DISPLAY_GUIDE.pdf

https://www.mouser.com/datasheet/2/302/AN13736-3073771.pdf?srsltid=AfmBOoobASIHe4SOtrDvchLUQZebrqyxV...

 

Regards

0 Kudos
Reply