Support for Ancillary Data in BT.656 streams?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for Ancillary Data in BT.656 streams?

1,313 Views
chrgrff1
Contributor II

Is it possible to access ancillary BT.656 data from i.MX6 IPU APIs?

We have an i.MX6 with a working 8-bit BT.656 input, and the video decoder chip is capable of adding vertical blanking interval data such as closed captioning to the BT.656 ancillary data stream. We'd like to take advantage of this.

I can't find anything hinting at support in the i.MX6DQ reference manual, but I'm hoping I'm missing something.

Thank you!

Labels (3)
0 Kudos
Reply
1 Reply

1,182 Views
igorpadykov
NXP Employee
NXP Employee

Hi chrgrff1

I am afraid there is no way to get ancillary data using 8-bit BT.656 input,

seems it could be possible using generic input format.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply