Support for Ancillary Data in BT.656 streams?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for Ancillary Data in BT.656 streams?

977件の閲覧回数
chrgrff1
Contributor II

Is it possible to access ancillary BT.656 data from i.MX6 IPU APIs?

We have an i.MX6 with a working 8-bit BT.656 input, and the video decoder chip is capable of adding vertical blanking interval data such as closed captioning to the BT.656 ancillary data stream. We'd like to take advantage of this.

I can't find anything hinting at support in the i.MX6DQ reference manual, but I'm hoping I'm missing something.

Thank you!

ラベル(3)
0 件の賞賛
返信
1 返信

845件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chrgrff1

I am afraid there is no way to get ancillary data using 8-bit BT.656 input,

seems it could be possible using generic input format.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信