An OpenCL program, derived from this Apple Developer example: OpenCL Parallel Reduction Example, fails with an accuracy error.
This program uses OpenCL to sum 1,048,576 floating point numbers 1000 times.
The program was run on imx6 quad with the arguments "gpu" and "float".
The imx6 is running Windows CE7 = WEC7 = Windows Embedded Compact 7.
Output:
Result[0] = 524317.562500 != 524315.912500
Error: Incorrect results obtained! Max error = 1.750000
The same OpenCL program, modified slightly to run on Windows 7/64 PC with an NIVIDIA K600, ran OK with no accuracy errors.
See attachments for the original OpenCL program source and derivatives.
The program has not been run on Linux. My hardware does not run Linux.
Original Attachment has been moved to: PC_AddUsingReduction.zip
Original Attachment has been moved to: WEC7_Add_UsingReduction.zip
Original Attachment has been moved to: Original-OpenCL_Parallel_Reduction_Example.zip
 
					
				
		
 andre_silva
		
			andre_silva
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I will test it on linux soon as possible.
regards,
Andre
 
					
				
		
 andre_silva
		
			andre_silva
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Andy,
please, find attached the ported code to imx6q sabresd board on Linux (yocto 3.10.53), also here are the results:
----------------------------------------------------------
root@imx6qsabresd:/home/fp_precision_test# ./reduce
----------------------------------------------------------------------
Connecting to Vivante Corporation Vivante OpenCL Device...
----------------------------------------------------------------------
Loading program 'reduce_int_kernel.cl'...
----------------------------------------------------------------------
Pass[ 0] Global[4096] Local[ 64] Groups[ 64] WorkItems[ 64] Operations[1] E]
Pass[ 1] Global[ 32] Local[ 32] Groups[ 1] WorkItems[ 32] Operations[1] E]
----------------------------------------------------------------------
Timing 1000 iterations of reduction with 1048576 elements of type int ...
----------------------------------------------------------------------
----------------------------------------------------------------------
Results Validated!
----------------------------------------------------------------------
root@imx6qsabresd:/home/fp_precision_test#
----------------------------------------------------------
Regards,
Andre
 
					
				
		
 andre_silva
		
			andre_silva
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Andy,
I am going to check that and let you know soon as possible.
regards,
Andre
Freescale does not support WinCE BSP for i.MX6.
Please apply to Adeneo.
Reference BSPs for Freescale i.MX6 SABRE LITE, SABRE SDB and SABRE SDP
Adeneo Embedded continues its commitment to support Freescale's i.MX roadmap
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------