Strange ONOFF Behaviour URGENT !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Strange ONOFF Behaviour URGENT !

6,518 Views
nachodiz
Contributor III

When pressing button 5 seconds, pmic goes off and inmediately goes on again

The correct behaviour should be to be off until new pressing its performed

Please see attached PDF Schematic Docs and help me

I need to start massive production just now! (50.000 pcs) near to $50 /pcb

mail: [email protected]

After 5sec pressing button, PMIC_ON_REQ goes down but it goes up again after 18ms

DSC_0074.JPG



DSC_0071.JPG


DSC_0072.JPG


King Regards


Labels (6)
0 Kudos
Reply
3 Replies

6,240 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Nacho,

 

Problem seems to be the configuration of the RESTARTEN bit (Bit 0) of the Power control register (PWRCTL), if this bit is set to “1”, the PF3001 restarts automatically after a power off event generated by the PWRON (held low for 4 seconds or longer) when PWR_CFG bit = 1. Make sure this bit is set to “0”.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,240 Views
nachodiz
Contributor III

Dear Jose

I´ve performed as you commented:

1 PMIC.png

2 pmic.png

3-pmic reg.png

It still fails but, the problem its not the PMIC, its the IMX6!

Because pmic goes off inmediately whrn PWRON its low (tested):

a.png
Please help us with this problem we have prodiuction stopped

If we dont fond the solution i PREPARED A VERSION that bypass the soc onoff stuffand perform the onoff function directly with the BIOS PIC MCU

2.png

:smileysad:


0 Kudos
Reply

6,240 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Hope the following helps.

https://community.nxp.com/message/843844 

Perhaps it is needed to have the SNVS voltage applied (say, from coin cell) 

to avoid the issue.

Regards,

Yuri.

0 Kudos
Reply