Hello Ran Shalit,
The UBOOT_CONFIG as qspi1 option references a specific defconfig file that configures the make instruction for compiling u-boot.
For example, this boot option for the i.MX6UL EVK calls the mx6ul_14x14_evk_qspi1_defconfig file which defines:
CONFIG_SYS_EXTRA_OPTIONS="IMX_CONFIG=board/freescale/mx6ul_14x14_evk/imximage.cfg,MX6UL,SYS_BOOT_QSPI"
CONFIG_ARM=y
CONFIG_TARGET_MX6UL_14X14_EVK=y
CONFIG_DM=y
CONFIG_DM_THERMAL=y
The easiest option then would be looking for the actual existing file for your board, since it’s already available.
There is no easy straightforward way to do this but you may look for references to this setting on the sources directory and look which defconfig is used for your board, for example with the command below:
$ grep -rnw '/<BSP_RELEASE_PATH>/sources/' -e "qspi1"
Then you would need to look for this file on the <BSP>/tmp/work directory.
I hope this helps!
Regards,