Splash screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Splash screen

2,722 Views
eishishibusawa
Contributor III

Dear Sir

 

I would like to display Splash screen from U-Boot to HDMI using i.MX6DL and L4.9.88_2.0.0.

 

I refer to the following community, but it seems that the Patch of Linux ver is a bit old one (L4.1.15_1.2.0).

https://community.nxp.com/docs/DOC-98109.

 

Q1.

Is there a patch for L 4.9.88 _ 2.0.0?

 

Best Regards,

Eishi SHIBUSAWA

 

Labels (4)
0 Kudos
Reply
2 Replies

2,578 Views
diegoadrian
NXP Employee
NXP Employee

Hello, 

Apparently, there is no patch for the newer Linux releases, and I do not know if there will be in the future. Since this depends on the engineer that create those patches. However, you can with professional service support and they can help you with the developer of the patch. I apologize for the inconveniences this could give you.

Best Regards,

Diego.  

0 Kudos
Reply

2,578 Views
eishishibusawa
Contributor III

Dear NXP support member

 

Please reply this question.

 

Best Regards,
Eishi SHIBUSAWA

0 Kudos
Reply