Splash screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Splash screen

2,726件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I would like to display Splash screen from U-Boot to HDMI using i.MX6DL and L4.9.88_2.0.0.

 

I refer to the following community, but it seems that the Patch of Linux ver is a bit old one (L4.1.15_1.2.0).

https://community.nxp.com/docs/DOC-98109.

 

Q1.

Is there a patch for L 4.9.88 _ 2.0.0?

 

Best Regards,

Eishi SHIBUSAWA

 

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,582件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello, 

Apparently, there is no patch for the newer Linux releases, and I do not know if there will be in the future. Since this depends on the engineer that create those patches. However, you can with professional service support and they can help you with the developer of the patch. I apologize for the inconveniences this could give you.

Best Regards,

Diego.  

0 件の賞賛
返信

2,582件の閲覧回数
eishishibusawa
Contributor III

Dear NXP support member

 

Please reply this question.

 

Best Regards,
Eishi SHIBUSAWA

0 件の賞賛
返信