Source code of "Fast Image Processing with i.MX6 Series (AN4629)" document

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source code of "Fast Image Processing with i.MX6 Series (AN4629)" document

3,064 Views
fikretalim
Contributor III

Hello,

I want to try the examples inside the document "Fast Image Processing with i.MX6 Series", but the codes inside the document are not completely given. Where can I find the source code for examples given in this document? Can you share if it is available?

Thanks

Fikret

0 Kudos
Reply
7 Replies

2,589 Views
wangziyou
Contributor I

i need the source code too.

0 Kudos
Reply

2,588 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can go to our official website to get it http://cache.nxp.com/files/32bit/doc/app_note/AN4629.pdf?fsrch=1&sr=1&pageNum=1 .

Have a nice day

Dan

0 Kudos
Reply

2,589 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Fikret,

Which source code do you want to get? All of our BSP are under the related i.MX products in freescale website.

Best Regards

Dan

0 Kudos
Reply

2,589 Views
fikretalim
Contributor III

Hi Dan,

I am looking for the source code of the examples given in the document AN4626. The link of the document is given below;

http://cache.freescale.com/files/32bit/doc/app_note/AN4629.pdf

I have already downloaded GPU SDK from the website, but this is not available inside it. Where can I find that?

Thanks,

Fikret


0 Kudos
Reply

2,588 Views
YixingKong
Senior Contributor IV

Fikret

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

2,588 Views
YixingKong
Senior Contributor IV

Fikret

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel free to contact Freescale.

Thanks,
Yixing

0 Kudos
Reply

2,588 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Fikret,

Do you mean gpu_sdk_v1.00.tar.gz? The link is http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&fpsp=1&tab=Design_Tools_Tab.It is under Snippets, Boot Code, Headers, Monitors, etc. (3)

pastedImage_1.png

Hope this can help you ~~

Best Regards

Dan

0 Kudos
Reply