Sony image sensor connection to imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sony image sensor connection to imx6

4,912 Views
erdani80
Contributor III

Hi,

 We are designing a board that will have two sony sensors and the image will be processed in an imx6.

 We are looking at solutions to convert from sub-lvds to parallel cmos interface.

 Has anybody a suggestion on a converter chip or solution we can use?, we are looking at a FPGA to do this but any comment is wellcomed.

Thanks,

  Daniel,

Labels (4)
Tags (3)
0 Kudos
Reply
7 Replies

2,904 Views
aneeshkumarvr
Contributor I

did you get any solution? thine has the chip sub-LVDS to parallel THC63LVD1024

0 Kudos
Reply

2,900 Views
erdani80
Contributor III

We used an FPGA and also implemented an ISP in the part.

4,317 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Daniel Amor,

There may be threads covering possible alternatives. FPGAs are certainly one, but it may be easier to use an available solution like the ADV7782.

http://www.analog.com/media/en/technical-documentation/data-sheets/ADV7782.pdf

I hope this helps!

Regards,

0 Kudos
Reply

4,317 Views
pks
Contributor I

Hello gusarambula,

I am curious whether you know if the ADV7782 not only supports the advertised OpenLDI LVDS, but also sub-LVDS which most Sony imaging sensors use. It seems like this might be the only alternative to using a Lattice FPGA solution.

0 Kudos
Reply

4,317 Views
erdani80
Contributor III

That could be an option, but we are targeting parallel camera sensor interface in the imx6 and this component uses serial MIPI.

I'll have a look at other analog parts, thanks :-)

0 Kudos
Reply

4,278 Views
jamiew
Contributor III

Hi @erdani80 

Did you ever find a device to do Sony LVDS to parallel MIPI on the i.MX6?

I need to do this as well.


Thanks

Jamie

0 Kudos
Reply

4,273 Views
erdani80
Contributor III

@jamiew , we placed an FPGA to do format conversion from sub LVDS to parallel video, and also some image processing to offload the processor