SoloX; How does MfgTool configure DDR3 interface for download?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SoloX; How does MfgTool configure DDR3 interface for download?

跳至解决方案
35,121 次查看
bap3ball
Contributor III

We have some custom hardware that is loosely based on the Sabre SD eval board and we are trying to use the MfgTool2 to program our Flash. Unfortunately the MfgTool2 is unable to boot any bootstrap images I've tried. The board is detected as a HID device and the MfgTool starts normally loading the various images but I am getting no indication the loaded u-boot image is booting on the hardware. There is no serial output and I have placed a GPIO toggle routine in the board_early_init section of u-boot and nothing is happening.

One difference between our hardware and the Sabre board is we use fly-by routing on the DDR3 interface, while it appears the Sabre uses point-point routing. I am guessing this may be causing the MfgTool to be unable to properly write into our DDR3 memories.

My understanding is the MfgTool loads images into the DDR memories and then boots from there. Is there some method to tell the MfgTool how to setup the DDR3 interface?

Any other reason one might guess on why the MfgTool fails to boot with the bootstrap images?

标签 (1)
0 项奖励
回复
1 解答
34,894 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Bruce

after running ddr test

i.MX6/7 DDR Stress Test Tool V2.51

new ddr settings obtained from test should be added to

uboot *.cfg file and mfg tools firmware rebuilt, using instructions

in attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
34,895 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Bruce

after running ddr test

i.MX6/7 DDR Stress Test Tool V2.51

new ddr settings obtained from test should be added to

uboot *.cfg file and mfg tools firmware rebuilt, using instructions

in attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

34,894 次查看
bap3ball
Contributor III

I tried that tool but get the following:

pastedImage_0.png

0 项奖励
回复
34,894 次查看
igorpadykov
NXP Employee
NXP Employee

suggest to create new thread as this is new question.

Best regards

igor

0 项奖励
回复