Software Upgrade through USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software Upgrade through USB

6,215 Views
kishorepoojari
Contributor III

Hello All,

           We are working on I.Mx233 processors and freescale provided B.S.P . As per the new requirement we have to upgrade the software through USB (previously we used SD card ).

Hence we have to implement all USB OTG diver in Bootloader ,

whether i.mx233 and freescale provided B.S.P will support for the same....?

Regards,

Kishore P

Labels (1)
0 Kudos
Reply
8 Replies

5,694 Views
igorpadykov
NXP Employee
NXP Employee

Hi kishore

in eboot one can download images to NAND with PB help, please

refer to attached WinCE Guide sect.5.5 Configuring USB Serial Connection

for Downloading and Debugging, sect.5.3.2 Burn EBOOT onto NAND flash using PB.

Otherwise one can use MFG Tools.

Best regards

igor

0 Kudos
Reply

5,694 Views
kishorepoojari
Contributor III

Hello igor,

   Problem with the our requirement is device will be fixed , we can't remove it for upgrade (If any update required) . Hence we are planning to implement USB OTG in the bootloader(whether it is possible in imx233 and win ce 6.0 ).

Regards,

Kishore P

0 Kudos
Reply

5,694 Views
igorpadykov
NXP Employee
NXP Employee

Hi kishore

USB OTG is supported in eboot bootloader

and usage is described in this document.

~igor

0 Kudos
Reply

5,694 Views
kishorepoojari
Contributor III

Hello igor,

  Please attach the document (USB OTG in eboot).

Regards,

Kishore P

0 Kudos
Reply

5,694 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kishore

it is attached in answer from

in general one can use eboot sources and write own custom application

for nand image update through usb.

0 Kudos
Reply

5,694 Views
YanjunLuo
Contributor IV

Hi Kishore,

Why not boot a Linux for upgrade? I did it for many years, it's much easier than bootloader.

Regards,

Yanjun Luo.

0 Kudos
Reply

5,694 Views
kishorepoojari
Contributor III

Hello Yanjun Luo,

  Current we are working on windows C.E 6.0 O.S ,  Is it possible that in Bootloader only device shall be USB OTG mode and copy the firmware from USB to NAND flash.

Regards,

Kishore P

0 Kudos
Reply

5,694 Views
YanjunLuo
Contributor IV

Hi Kishore,

Sorry I know nothing about WINCE.

Regards,

Yanjun Luo.

0 Kudos
Reply