Software Upgrade through USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software Upgrade through USB

6,586件の閲覧回数
kishorepoojari
Contributor III

Hello All,

           We are working on I.Mx233 processors and freescale provided B.S.P . As per the new requirement we have to upgrade the software through USB (previously we used SD card ).

Hence we have to implement all USB OTG diver in Bootloader ,

whether i.mx233 and freescale provided B.S.P will support for the same....?

Regards,

Kishore P

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

6,065件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kishore

in eboot one can download images to NAND with PB help, please

refer to attached WinCE Guide sect.5.5 Configuring USB Serial Connection

for Downloading and Debugging, sect.5.3.2 Burn EBOOT onto NAND flash using PB.

Otherwise one can use MFG Tools.

Best regards

igor

0 件の賞賛
返信

6,065件の閲覧回数
kishorepoojari
Contributor III

Hello igor,

   Problem with the our requirement is device will be fixed , we can't remove it for upgrade (If any update required) . Hence we are planning to implement USB OTG in the bootloader(whether it is possible in imx233 and win ce 6.0 ).

Regards,

Kishore P

0 件の賞賛
返信

6,065件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kishore

USB OTG is supported in eboot bootloader

and usage is described in this document.

~igor

0 件の賞賛
返信

6,065件の閲覧回数
kishorepoojari
Contributor III

Hello igor,

  Please attach the document (USB OTG in eboot).

Regards,

Kishore P

0 件の賞賛
返信

6,065件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kishore

it is attached in answer from

in general one can use eboot sources and write own custom application

for nand image update through usb.

0 件の賞賛
返信

6,065件の閲覧回数
YanjunLuo
Contributor IV

Hi Kishore,

Why not boot a Linux for upgrade? I did it for many years, it's much easier than bootloader.

Regards,

Yanjun Luo.

0 件の賞賛
返信

6,065件の閲覧回数
kishorepoojari
Contributor III

Hello Yanjun Luo,

  Current we are working on windows C.E 6.0 O.S ,  Is it possible that in Bootloader only device shall be USB OTG mode and copy the firmware from USB to NAND flash.

Regards,

Kishore P

0 件の賞賛
返信

6,065件の閲覧回数
YanjunLuo
Contributor IV

Hi Kishore,

Sorry I know nothing about WINCE.

Regards,

Yanjun Luo.

0 件の賞賛
返信