Slow camera display using opencv on i.MX8mPlus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Slow camera display using opencv on i.MX8mPlus

ソリューションへジャンプ
1,796件の閲覧回数
frk
Contributor III

Hi,

 

I'm currently trying to use OpenCV with a mipi camera on i.MX8mPlus.

The goal is to display the video stream of the camera and interact with it through OpenCV (ie: pattern detection).

My main interrogation is about the video display that is very laggy.

Using Gstreamer or QT5 to display the camera stream, everything is smooth but using OpenCV add delay and lag.

Is there any way to accelerate OpenCV through the GPU or something else?

0 件の賞賛
返信
1 解決策
1,789件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello frk,

IF you are connecting to mipi you must get at least 10fps with opencv if not then you must modify the driver, current driver are for mipi camera on OV5640 and OV2281.

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,790件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello frk,

IF you are connecting to mipi you must get at least 10fps with opencv if not then you must modify the driver, current driver are for mipi camera on OV5640 and OV2281.

Regards

 

0 件の賞賛
返信