Single x32 DDR3 Module for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Single x32 DDR3 Module for i.MX6

跳至解决方案
2,912 次查看
cayt
Contributor II

Hi,

I am busy sketching a system draft using i.MX6DL with x32bit DDR3 memory. As far as my research goes only the LPDDR3 memories have x32 bit data width but unfortunately i.MX6 devices don't support LPDDR3. The DDR3 and LVDDR3 memories have x16 bit data width only. I know I could use 2 LV/DDR3 modules but space is one of the biggest challenges in the design, that's why I would like to keep it to a single memory module, if possible. Could anyone suggest a direction to go?

Thanks!

标签 (2)
标记 (4)
0 项奖励
回复
1 解答
2,444 次查看
cayt
Contributor II

Hi,

By mistake I opened the same discussion twice. Please leave your comments on this discussion

Thanks,

Cahit

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,445 次查看
cayt
Contributor II

Hi,

By mistake I opened the same discussion twice. Please leave your comments on this discussion

Thanks,

Cahit

0 项奖励
回复
2,444 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Cahit

for space constrained designs it may be useful to look at scm modules

http://www.nxp.com/scm

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,444 次查看
cayt
Contributor II

Hi Igor,

Thanks for the suggestion. I am aware of these chips but the memory technology used is LPDDR2 and I have to use DDR3. BTW, I see that the PMIC MMPF0100 is integrated in the chip. Are there any heat issues with these chips, that you are aware of?

Thanks,

Cahit

0 项奖励
回复