Single Camera output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single Camera output

1,158 Views
deepanrajanbara
Contributor IV

Hi

We are currently working on imx6 with Linux kernel .As we require to capture video from one camera and use the same video for displaying in another board at the same time on the current board .so multiple output with single camera .Is it possible .if so what are the software changes to be done in Kernel level .

Thank you,

Deepanraj.A

Tags (1)
0 Kudos
Reply
1 Reply

1,017 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Deeparaj,

Please take a look at this thread,

Re: IPU multiple video out + Overlay


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply