Signing Linux kernel (5.4.3-2.0.0) problem on iMX8QXP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Signing Linux kernel (5.4.3-2.0.0) problem on iMX8QXP

4,271 次查看
MistX
Contributor III

Hello!

Have a trouble with signing Linux kernel images for iMX8QXP.

Image generation and sign passes without errors. I`m using guide - https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/ahab/guides/mx8_mx8x_secure_boot.t... to sign Linux kernel image.

Tools:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.139-0-g1a8f760

UBOOT builded with AHAB support - U-Boot 2019.04mmv_14-07-2021 (Jul 14 2021 - 18:39:06 +0300) Kontron SMARC-sAMX8X   Release develop aarch64-linux-gnu-gcc (Ubuntu 9.3.0-17ubuntu1~20.04) 9.3.0 GNU ld (GNU Binutils for Ubuntu) 2.34 (uboot_samx8x-R13 - BSP)

https://source.codeaurora.org/external/imx/imx-mkimage (imx_5.4.3_2.0.0)

imx-scfw-porting-kit-1.4.0

imx-seco-3.7.5

https://source.codeaurora.org/external/imx/imx-atf.git (imx_5.4.3_2.0.0)

Code Signing Tool release version 3.2.0 (Ubuntu 20.04.2 repository package)

Linux kernel image - SMARC-sAMX8X_Yocto-BSP_R13/images.tar/images/Image (5.4.3-2.0.0+g1675c67c9170)

CSF:

破坏者

[Header]
Target = AHAB
Version = 1.0

[Install SRK]
# SRK table generated by srktool
File = "../SRK_1_2_3_4_table.bin"
# Public key certificate in PEM format
Source = "../crts/SRK1_sha384_secp384r1_v3_ca_crt.der"
# Index of the public key certificate within the SRK table (0 .. 3)
Source index = 0
# Type of SRK set (NXP or OEM)
Source set = OEM
# bitmask of the revoked SRKs
Revocations = 0x0

[Install Certificate]
# Public key certificate in PEM or DER format
File = "../crts/SGK1_1_sha384_secp384r1_v3_usr_crt.der"
Permissions = 0x1

[Authenticate Data]
# Binary to be signed generated by mkimage
File = "flash.bin"
# Offsets = Container header Signature block (printed out by mkimage)
Offsets = 0x0 0x110

If to parse resulting signed Image (mkimage_imx8 --soc=QX --parse=Image.signed) everything looks OK:

破坏者
SOC: QX  
Input container binary to be parsed: Image.signed
CONTAINER FUSE VERSION: 0x00
CONTAINER SW VERSION:   0x0000

*********************************
*                               *
*          CONTAINER 1          *
*                               *
*********************************

       Length: 0X420 (1056)
          Tag: 0X87
      Version: 0
        Flags: 0X2
   Num images: 2
 Fuse version: 0
   SW version: 0
Sig blk offset: 0X110

IMAGE 1 (Bootloader)
Offset: 0X2000                                                                                                                                                                                                                                                                            
Size: 0X1AE7400 (28210176)                                                                                                                                                                                                                                                                
Load Addr: 0X80280000                                                                                                                                                                                                                                                                     
Entry Addr: 0X80280000                                                                                                                                                                                                                                                                    
Flags: 0X143 (IMG TYPE: Executable | CORE ID: CORE_CA53 | HASH TYPE: SHA384 | ENCRYPTED: NO)                                                                                                                                                                                              
Metadata: 0X1355FC                                                                                                                                                                                                                                                                        
Hash: 96fbf2e504d3a2ca3b1b887c2695029ba630c137ade7446bf94dcfdede27a1b87974751773c6635006a1cbcf1b67959c (SHA384)                                                                                                                                                                           
                                                                                                                                                                                                                                                                                         
IMAGE 2 (Data)                                                                                                                                                                                                                                                                            
Offset: 0X1AE9400                                                                                                                                                                                                                                                                         
Size: 0X17000 (94208)                                                                                                                                                                                                                                                                     
Load Addr: 0X83000000                                                                                                                                                                                                                                                                     
Entry Addr: 0                                                                                                                                                                                                                                                                             
Flags: 0X144 (IMG TYPE: Data | CORE ID: CORE_CA53 | HASH TYPE: SHA384 | ENCRYPTED: NO)                                                                                                                                                                                                    
Metadata: 0                                                                                                                                                                                                                                                                               
Hash: 80701691b3a4457fd729b0d2d7db88600fff3d0eb1739c88660230fa2521d803240091ad2e299962678e0e8ddabd6764 (SHA384)

But when I try to check secure boot on SD card with written signed kernel using

 

破坏者

sudo ~/bin/uuu sd_flash.signed.bin

IN UBOOT:

=> run loadimage

=> auth_cntr ${loadaddr}

 I`m getting error:

Authenticate OS container at 0x80280000  
Error: Wrong container header

破坏者
=> iminfo                

## Checking Image at 80280000 ...
Unknown image format!

AHAB:

破坏者
=> ahab_status  
Lifecycle: 0x0020, NXP closed

sc_seco_get_event: idx: 0, res:3
No SECO Events Found!

What am I doing wrong?

标记 (1)
0 项奖励
回复
6 回复数

4,130 次查看
Yuri
NXP Employee
NXP Employee

@MistX 
Hello,

   also, please use app note AN12312: Secure Boot on i.MX 8 and i.MX 8X Families using AHAB

https://www.nxp.com/webapp/Download?colCode=AN12312

 

Regards,
Yuri.

0 项奖励
回复

4,219 次查看
Yuri
NXP Employee
NXP Employee

@MistX 
Hello,

  I've sent You some comments.

Regards,
Yuri.

0 项奖励
回复

4,185 次查看
MistX
Contributor III

Unfortunately, It does not help.

0 项奖励
回复

4,251 次查看
MistX
Contributor III

Are there any special uboot build options (not described in docs) for loading signed Linux images?

0 项奖励
回复

4,254 次查看
MistX
Contributor III

Ok, I have changed the SD-card, but it helped a little.

I can`t boot or auth signed Linux image.

破坏者
=> run sdboot
Booting from SD card ...
Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
28082176 bytes read in 630 ms (42.5 MiB/s)
93947 bytes read in 12 ms (7.5 MiB/s)
Bad Linux ARM64 Image magic!

=> run loadimage
28082176 bytes read in 614 ms (43.6 MiB/s)
=> iminfo        

## Checking Image at 80280000 ...
Unknown image format!
=> auth_cntr ${loadaddr}
Authenticate OS container at 0x80280000  
"Synchronous Abort" handler, esr 0x96000147
elr: 0000000080021548 lr : 0000000080025d10 (reloc)
elr: 00000000ffe8b548 lr : 00000000ffe8fd10
x0 : 0000000000000000 x1 : 0000000000000040
x2 : 0000000000000040 x3 : 000000000000003f
x4 : 0000000081d35400 x5 : 0000000000000020
x6 : 00000000ffebc83c x7 : 00000000fd676690
x8 : 00000000fd676658 x9 : 0000000000000008
x10: 00000000ffffffd0 x11: 0000000000000010
x12: 0000000000000000 x13: 0000000000000200
x14: 0000000000000000 x15: 0000000000000020
x16: 00000000ffebc83c x17: 0000000000000000
x18: 00000000fd687d98 x19: 0000000080280010
x20: 00000000fff1a708 x21: 0000000080280000
x22: 0000000000000000 x23: 00000000fff0077f
x24: 0000000000000002 x25: 0000000000000000
x26: 0000000000000000 x27: 0000000000000000
x28: 00000000fd6b9330 x29: 00000000fd676630

Resetting CPU ...

### ERROR ### Please RESET the board ###
0 项奖励
回复

4,263 次查看
MistX
Contributor III

Also found that Linux image actualy does not load with load command in uboot. May be problem with SD-card driver in uboot...

=> run loadimage                                                  
** fs_devread read error - block

SD Card - Samsung EVO Plus 64Gb

=> mmc info
Device: FSL_SDHC
Manufacturer ID: 1b
OEM: 534d
Name: EC1S5  
Bus Speed: 50000000
Mode : SD High Speed (50MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 59.7 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes

=> ext4ls mmc 1:1 /boot
<DIR>       4096 .
<DIR>       4096 ..
          93547 kontron-samx8x-dxp.dtb
       27935232 Image-5.4.3-2.0.0+gf0616714e7cf
<SYM>         12 Image
          93963 kontron-samx8x-qxp-m4.dtb
          93947 kontron-samx8x-qxp.dtb
          92535 kontron-samx8x-dx-m4.dtb
          93563 kontron-samx8x-dxp-m4.dtb
          92519 kontron-samx8x-dx.dtb
       28312576 Image.signed

0 项奖励
回复