SharedFdPipe.cpp in OpenMAXIL/src/content_pipe/shared_fd_pipe generates illegal seek error when socket or pipe is used as output of Andriod media recorder

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SharedFdPipe.cpp in OpenMAXIL/src/content_pipe/shared_fd_pipe generates illegal seek error when socket or pipe is used as output of Andriod media recorder

2,146 次查看
mjoa
Contributor II

Hi,

is it possible to stream output from Android media recorder using socket or pipe to another NDK application on the same i.MX device that in turn streams it out? I have tried the followings to set outputfile of media recorder:

// recorder.setOutputFile("/data/data/com.persistentsystems.videocast/files/pipe0"); //pipe

//            recorder.setOutputFile(pfd.getFileDescriptor()); //socket

            recorder.setOutputFile("/sdcard/test_video.mp4"); //file

SharedFdPipe.cpp (proprietary code of Freescale) in OpenMAXIL/src/content_pipe/shared_fd_pipe generates illegal seek error when socket or pipe is used

as output of Mediarecorder:

02-11 21:53:14.560 I/OMXPlayer( 3658): LEVEL: 1 FUNCTION: SharedFdPipe_Open LINE: 39

02-11 21:53:14.560 I/OMXPlayer( 3658): SFD open sharedfd://28:0:0

02-11 21:53:14.560 I/OMXPlayer( 3658): LEVEL: 1 FUNCTION: SharedFdPipe_Open LINE: 59

02-11 21:53:14.560 I/OMXPlayer( 3658): seek to pos: 0 failed, errno: Illegal seek

When file is used as output of media recorder, recording could be done successfully:

02-11 22:01:20.820 I/OMXPlayer( 4603): LEVEL: 1 FUNCTION: SharedFdPipe_Open LINE: 39

02-11 22:01:20.820 I/OMXPlayer( 4603): SFD open sharedfd://28:0:0

02-11 22:01:20.830 I/vpu-lib ( 4603): <gpu> alloc handle: 0x4c3f4cc0, paddr: 0x3e1df000, vaddr: 0x4a113000

02-11 22:01:20.830 I/xx      ( 4841): C

02-11 22:01:20.830 I/OMXPlayer( 4603): start recorder.

Thank you so much for your help.

标签 (3)
0 项奖励
回复
2 回复数

1,910 次查看
mjoa
Contributor II

Could GMRecorder::setOutputFileFD be modified NOT to use sharedfd for gm_path

sprintf(gm_path, "sharedfd://%d:%lld:%lld",  mSharedFd, offset, length);

but to use  UdpsPipe? Should it be?

sprintf(gm_path, "udp://%d:%lld:%lld",  mSharedFd, offset, length);

0 项奖励
回复

1,910 次查看
mjoa
Contributor II

After modifying to use UdpsPipe in GMRecorder::setOutputFileFD

     sprintf(gm_path, "udp://%d:%lld:%lld",  mSharedFd, offset, length);

and to use udp socket fd in setOutputFile

     recorder.setOutputFile(pfd.getFileDescriptor()); //socket

crash appears as follow:

02-12 18:03:32.337 I/vpu-lib ( 4623): <gpu> alloc handle: 0x415945a8, paddr: 0x38710000, vaddr: 0x4572c000

02-12 18:03:32.337 I/vpu-lib ( 4623): ringBufferEnable 0, chromaInterleave 1, mapType 1, linear2TiledEnable 1

02-12 18:03:32.337 F/libc    ( 4623): @@@ ABORTING: invalid address or address of corrupt block 0x4164d460 passed to dlfree

02-12 18:03:32.337 F/libc    ( 4623): Fatal signal 11 (SIGSEGV) at 0xdeadbaad (code=1), thread 5099 (mediaserver)

02-12 18:03:32.347 I/vpu-lib ( 4623): <gpu> alloc handle: 0x415945c0, paddr: 0x3e019000, vaddr: 0x4b035000

02-12 18:03:32.667 I/DEBUG   ( 2416): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***

02-12 18:03:32.667 I/DEBUG   ( 2416): Build fingerprint: 'waverelay/full_mpu5/mpu5:4.3/JSS15J/eng.jbodino.20141020.101151:user/dev-keys'

02-12 18:03:32.667 I/DEBUG   ( 2416): Revision: '405522'

02-12 18:03:32.667 I/DEBUG   ( 2416): pid: 4623, tid: 5099, name: mediaserver  >>> /system/bin/mediaserver <<<

02-12 18:03:32.667 I/DEBUG   ( 2416): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr deadbaad

02-12 18:03:32.667 I/DEBUG   ( 2416): Abort message: '@@@ ABORTING: invalid address or address of corrupt block 0x4164d460 passed to dlfree'

02-12 18:03:32.677 W/NativeCrashListener( 2714): Couldn't find ProcessRecord for pid 4623

02-12 18:03:32.767 I/DEBUG   ( 2416):     r0 00000027  r1 00000000  r2 00000008  r3 deadbaad

02-12 18:03:32.767 I/DEBUG   ( 2416):     r4 00000000  r5 4e0ea974  r6 4000b000  r7 4164d468

02-12 18:03:32.767 I/DEBUG   ( 2416):     r8 40e49218  r9 410c4237  sl 8000100e  fp 40e4c2b8

02-12 18:03:32.767 I/DEBUG   ( 2416):     ip 00000001  sp 4e0ea970  lr 4021e12b  pc 4021b684  cpsr 60070030

02-12 18:03:32.767 I/DEBUG   ( 2416):     d0  0000000000000000  d1  0000000000000000

02-12 18:03:32.767 I/DEBUG   ( 2416):     d2  0000000000000000  d3  0000000000000000

02-12 18:03:32.767 I/DEBUG   ( 2416):     d4  3fcaa1a0953f52d4  d5  bebbb74342c19da4

02-12 18:03:32.767 I/DEBUG   ( 2416):     d6  3e66376972bea4d0  d7  3f80000080cd85cf

02-12 18:03:32.767 I/DEBUG   ( 2416):     d8  0000000000000000  d9  0000000000000000

02-12 18:03:32.767 I/DEBUG   ( 2416):     d10 0000000000000000  d11 0000000000000000

02-12 18:03:32.767 I/DEBUG   ( 2416):     d12 0000000000000000  d13 0000000000000000

02-12 18:03:32.777 I/DEBUG   ( 2416):     d14 0000000000000000  d15 0000000000000000

02-12 18:03:32.777 I/DEBUG   ( 2416):     d16 3fa1cbc4e2559733  d17 0000000000000000

02-12 18:03:32.777 I/DEBUG   ( 2416):     d18 0000000000000000  d19 bfc781bb09000000

02-12 18:03:32.777 I/DEBUG   ( 2416):     d20 3fc5524416f6467c  d21 bf66bcbf933eb23c

02-12 18:03:32.777 I/DEBUG   ( 2416):     d22 bfc839d0ffa746ac  d23 3fd0000000000000

02-12 18:03:32.777 I/DEBUG   ( 2416):     d24 3f9041eae95bdec5  d25 bf9041eaefea5a92

02-12 18:03:32.777 I/DEBUG   ( 2416):     d26 3f6328e1cb8c85e0  d27 4000000000000000

02-12 18:03:32.777 I/DEBUG   ( 2416):     d28 4001839d0ffa746b  d29 3fc5797dab02b4ae

02-12 18:03:32.777 I/DEBUG   ( 2416):     d30 3ff0000000000000  d31 3fcaa1a0953f52d4

02-12 18:03:32.777 I/DEBUG   ( 2416):     scr 68000010

02-12 18:03:32.787 I/DEBUG   ( 2416):

02-12 18:03:32.787 I/DEBUG   ( 2416): backtrace:

02-12 18:03:32.787 I/DEBUG   ( 2416):     #00  pc 0001e684  /system/lib/libc.so

02-12 18:03:32.787 I/DEBUG   ( 2416):     #01  pc 0001c550  /system/lib/libc.so (abort+4)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #02  pc 000121f1  /system/lib/libc.so

02-12 18:03:32.787 I/DEBUG   ( 2416):     #03  pc 00010ea1  /system/lib/libc.so (dlfree+1184)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #04  pc 0000d9df  /system/lib/libc.so (free+10)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #05  pc 00001f53  /system/lib/lib_omx_osal_v2_arm11_elinux.so (fsl_osal_dealloc+2)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #06  pc 0000548d  /system/lib/lib_mp4_muxer_arm11_elinux.so

02-12 18:03:32.787 I/DEBUG   ( 2416):     #07  pc 000052cb  /system/lib/lib_mp4_muxer_arm11_elinux.so (MP4DeleteMuxer+22)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #08  pc 0000540f  /system/lib/lib_mp4_muxer_arm11_elinux.so (MP4CreateMuxer+150)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #09  pc 00001ecf  /system/lib/lib_omx_fsl_muxer_v2_arm11_elinux.so (FslMuxer::InitMuxer()+34)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #10  pc 0001b4ad  /system/lib/lib_omx_common_v2_arm11_elinux.so (Muxer::InstanceInit()+76)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #11  pc 0000d077  /system/lib/lib_omx_common_v2_arm11_elinux.so (IdleState::ToExecuting()+10)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #12  pc 0000ece7  /system/lib/lib_omx_common_v2_arm11_elinux.so (State::ProcessCmd()+134)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #13  pc 0000ca17  /system/lib/lib_omx_common_v2_arm11_elinux.so (DoThread(void*)+138)

02-12 18:03:32.787 I/DEBUG   ( 2416):     #14  pc 0000ca78  /system/lib/libc.so (__thread_entry+72)

02-12 18:03:32.797 I/DEBUG   ( 2416):     #15  pc 0000cbf4  /system/lib/libc.so (pthread_create+208)

Any good suggestion? Thank you so much,

0 项奖励
回复