Setting static random address for bluetooth in Android 9.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting static random address for bluetooth in Android 9.0

ソリューションへジャンプ
2,440件の閲覧回数
asmaa
Contributor V

Hello Everyone,

We are using IMX7D with android 9.0 in our product with a 1MW module. I want to set a static random address for the Bluetooth

How can this be achieved in android 9.0(uboot or kernel), can someone please shed some light on it?

@Yuri  

Thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
2,423件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately the setup it is related to the Firmware of the Module, so please contact Murata ( module Maker of the Bluetooth)  to get the information about the driver, to make the configuration in other devices usually there is a config file for this purposes. But I really do not know with this Cypress device, and it is better to contact with Murata, to see what features they are offering.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,424件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately the setup it is related to the Firmware of the Module, so please contact Murata ( module Maker of the Bluetooth)  to get the information about the driver, to make the configuration in other devices usually there is a config file for this purposes. But I really do not know with this Cypress device, and it is better to contact with Murata, to see what features they are offering.

 

0 件の賞賛
返信