Setting fb other than fb0 as a primary

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting fb other than fb0 as a primary

2,822 次查看
ambika
Contributor II

Hii,

I'm working on imx6q processor with yocto dizzy(linux kernel 3.14).

Currently the data is writing to /dev/fb0 and from there to my primary display through the first LVDS channel  (LVDS0).

ldb node in dtsi is as below,

...

...

&ldb {
status = "okay";

lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <18>;
primary;
crtc = "ipu1-di0";
status = "okay";

display-timings {
native-mode = <&timing0>;
timing0: ldb-wvga {
clock-frequency = <33260000>;
hactive = <800>;
vactive = <480>;
hback-porch = <88>;
hfront-porch = <40>;
vback-porch = <33>;
vfront-porch = <10>;
hsync-len = <128>;
vsync-len = <2>;
};
};
};
};

...

...

From u-boot mxcfb0 tis set to primary display

I assume that currently the data write will be to ipu1_di0 i.e /dev/fb0 and that fb0 is configured to display.

I want to achieve the following,

  1. Write the data to other than ipu1_di0 (if possible to virtual frame buffer) say to fbx.
  2. From fbx to fb0 (on doing some operations like scaling on data in fbx to fb0)

Configuration /dev/fb0 to display is okey.

Please let know the procedure to achieve (1)

Thanks in advance.

Regards,

Ambika

0 项奖励
回复
2 回复数

2,519 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复

2,519 次查看
ambika
Contributor II

hello Bio_TICFSL,

Thanks for the links.

But I want to take the data which is going to the fb0 to virtual frame buffer (fb5) and then do scaling on the data and then send it to fb0.

i.e I want to dump the modified data on my display instead of directly dumping it on the display.

Is there any clue to achieve the same. I'm not able to get where the data is captured to fb0 in my original source code.

Thanks in advance.

Regards,

Ambika

0 项奖励
回复