Set asrc input clock to SPDIF_RX_CLK on IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Set asrc input clock to SPDIF_RX_CLK on IMX6

ソリューションへジャンプ
2,768件の閲覧回数
manuel_soledge
Contributor II

Hi,

I am working on an audio application using an i.MX6ULL and I need to use the hardware ASRC of the processor with the S/PDIF RX clock on the asrc pair input.

The problem I have I that even after the S/PDIF dpll is locked I can't read the rate of the spdif_rx_clk so the pair configuration fails to calculate the input divisor.

In the reference manual I read that after the spdif dpll is locked the received rate is directly generated to spdif_rx_clk. Is that right or are there registers to configure to make it go through to the asrc controller?

Thank you,

Manuel BA

ラベル(2)
1 解決策
2,655件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

S/PDIF RX clock is described in sect.50.4.1.8 

i.MX 6ULL Applications Processor Reference Manual

pastedImage_1.jpg

some spdif tests which may be useful:

doc\mxc_spdif_test\test - imx-test - i.MX Driver Test Application Software 

doc\mxc_asrc_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,656件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

S/PDIF RX clock is described in sect.50.4.1.8 

i.MX 6ULL Applications Processor Reference Manual

pastedImage_1.jpg

some spdif tests which may be useful:

doc\mxc_spdif_test\test - imx-test - i.MX Driver Test Application Software 

doc\mxc_asrc_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,655件の閲覧回数
manuel_soledge
Contributor II

Hi,

Thank you for your answer, I have been able to recover the RX clock in the asrc module.
I also have opened another question about the asrc clock sources.

Manuel

0 件の賞賛
返信