Set Mac address on imx233

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set Mac address on imx233

1,194 Views
PramodKumar
Contributor IV

Please guide ,how to set mac address permanently through kernel in imx233 board.

Thanks

Pramod Kumar

Labels (7)
0 Kudos
Reply
1 Reply

1,002 Views
igorpadykov
NXP Employee
NXP Employee

HI Pramod

one can try in Uboot setup board mac address, like:

U-Boot> setenv ethaddr 00:04:9F:00:EA:D7

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply