Cannot download BSP 3.10.17 (Yocto)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot download BSP 3.10.17 (Yocto)

3,321件の閲覧回数
faisaltaj
Contributor II

Hi,

I have wasted plenty of time trying to work around a way to get through this problem. I am exactly following Freescale_Yocto_Project_User's_Guide.pdf instructions to get hold of Yocto Project layers but no matter what I do, end result is always same:

after configuring git with name and email add:

I executed this:

ubuntu@ubuntu:$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.17-1.0.2_ga

result:

fatal: cannot obtain manifest git://git.freescale.com/imx/fsl-arm-yocto-bsp.git

Yes I am behind proxy server. One solution I found looking around was to configure git with further parameters:

git config --global http.proxy http://proxyuser:proxypwd@proxy.server.com:8080proxypwd@proxy.server.com:8080

git config --global https.proxy https://proxyuser:proxypwd@proxy.server.com:8080proxypwd@proxy.server.com:8080

did that too, but still the same result.

Have anyone before had faced this scenario? Please help when you got it fixed.

Thanking in advance.

Faisal

ラベル(3)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,082件の閲覧回数
franckmaillot
Contributor I

Hello,

use http://git.freescale.com/git/cgit.cgi/imx/whatever.git instead. It looks like a cgi script is used to give you access to the git repository over http.

git config http_proxy is still required.

Regards,

Franck

0 件の賞賛
返信

2,082件の閲覧回数
rodrigoaldana
Contributor I

Hi Faisal,

I think the problem the problem is in your proxy configuration,

You might find this link useful:

https://wiki.yoctoproject.org/wiki/Working_Behind_a_Network_Proxy

Regards,

Rodrigo

2,082件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

rodrigoaldana, would you please help on this?

0 件の賞賛
返信