Serial Downloader Mode in i.MX RT1050 EVKB from Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Serial Downloader Mode in i.MX RT1050 EVKB from Application

1,415 次查看
anshulkhare
Contributor III

Hello All,

i am working on IMX RT-1050 EVKB board, i am trying to run serial downloader mode from application(SW). through hardware pin settings i am able to run serial Downloader mode. but i need to run it from application. can anyone help me on this.

Regards,

Anshul

标记 (1)
0 项奖励
回复
2 回复数

1,385 次查看
anshulkhare
Contributor III

@EdwinHzThanks For your reply.

from application i want to enter into boot mode,to communicate with Boot ROM code.

as of now this problem got resolved, i am able to enter into boot mode from application, i have followed the Reference manual Section "9.13.3".

Regrads,

Anshul

0 项奖励
回复

1,400 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @anshulkhare,

Switching between boot modes has to be done from hardware (using fuses and/or GPIOs) by design, since deciding the boot mode is part of the boot sequence that the MCU undergoes immediately after a reset. Therefore it is not possible to switch boot modes from application.

 

BR,

Edwin.

0 项奖励
回复