Selecting a suitable i.MX6 development board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Selecting a suitable i.MX6 development board

Jump to solution
1,728 Views
afzalmohammed
Contributor I

Hi,

I have a requirement - a new WiFi device that can be connected through full size MMC/SD connector, needs to work in Linux on an i.MX6 platform. WiFi device also has an alternate mode of communicating through UART.

Hardware requirements on development board,

1. full size MMC/SD slot (for connecting WiFi device)

2. Another full size MMC/SD or microSD slot - for the card with images for booting

3. debug UART

4. UART with flow control capabilities (for WiFi device at higher speed)

5. at least one LED that can be controlled via GPIO

6. USB OTG

In software side, it would need to run DHCP, http server etc. on Linux, so may be an Ubuntu.

Please suggest an i.MX6 development board that suits above hardware requirements and on which software sources (& support) are available so that we can quickly start developing WiFi driver.

Note: I am new to Freescale things

Regards

Afzal

Labels (2)
0 Kudos
Reply
1 Solution
1,589 Views
igorpadykov
NXP Employee
NXP Employee

Hi, Afzal I believe Sabre Automotive board will most

suit for these purposes

SABRE for Automotive Infotainment Based on the i.MX 6 Series

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,590 Views
igorpadykov
NXP Employee
NXP Employee

Hi, Afzal I believe Sabre Automotive board will most

suit for these purposes

SABRE for Automotive Infotainment Based on the i.MX 6 Series

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply