Seiko Touch shows no display with IMX53 Linux start-R board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Seiko Touch shows no display with IMX53 Linux start-R board

ソリューションへジャンプ
4,831件の閲覧回数
swaraj
Contributor II

Hi,

Nothing is seen on seiko display (touch), when trying to boot IMX53-Ubuntu on start-R board. Can anybody help me in displaying GUI on touch. I'm able to display the GUI through VGA.

Thanks

Swaraj

ラベル(2)
0 件の賞賛
返信
1 解決策
4,532件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For the Seiko display, please try to add the "video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary" in the bootargs in u-boot.

Basically, you can check the BSP release note for all the bootargs parameters for kernel boot.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,533件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For the Seiko display, please try to add the "video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary" in the bootargs in u-boot.

Basically, you can check the BSP release note for all the bootargs parameters for kernel boot.

0 件の賞賛
返信
4,532件の閲覧回数
swaraj
Contributor II

Hi Chin Fung Chan,

Thanks a lot. It worked for me. Now i have an other issue. Currently i'm using Ubuntu on IMX53, how should i enable virtual keyboard at login and for typing.

0 件の賞賛
返信
4,532件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think you talk about the on-screen keyboard. I didn't try it on the i.MX board. but I think the following information may useful for you.

1. http://cmwelsh.com/enable-on-screen-keyboard-ubuntu-lucid-lynx

2. http://ubuntuforums.org/showthread.php?t=1392583

4,532件の閲覧回数
RandyKrakora
NXP Employee
NXP Employee

Did you see this yet?

https://community.freescale.com/message/228134#228134

Regards,

Randy

0 件の賞賛
返信
4,532件の閲覧回数
swaraj
Contributor II

Hi Randy,

     I have IMX53 Start-R board with the following information on the board:  SCH -27104 Rev B 700-27104 Rev X5. The link you have specified talks about the IMX53 QSB board.

Do we really need to do any modification on this version of Start-R boards to get the display. Please let us know.

Thanks,

Swaraj,

0 件の賞賛
返信
4,532件の閲覧回数
RandyKrakora
NXP Employee
NXP Employee

What are your uboot args?

Regards,

Randy Krakora

Field Applications Engineer

Freescale Semiconductor

(765)-860-6622

0 件の賞賛
返信