Seiko Touch shows no display with IMX53 Linux start-R board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Seiko Touch shows no display with IMX53 Linux start-R board

跳至解决方案
4,814 次查看
swaraj
Contributor II

Hi,

Nothing is seen on seiko display (touch), when trying to boot IMX53-Ubuntu on start-R board. Can anybody help me in displaying GUI on touch. I'm able to display the GUI through VGA.

Thanks

Swaraj

标签 (2)
0 项奖励
回复
1 解答
4,515 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For the Seiko display, please try to add the "video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary" in the bootargs in u-boot.

Basically, you can check the BSP release note for all the bootargs parameters for kernel boot.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,516 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For the Seiko display, please try to add the "video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary" in the bootargs in u-boot.

Basically, you can check the BSP release note for all the bootargs parameters for kernel boot.

0 项奖励
回复
4,515 次查看
swaraj
Contributor II

Hi Chin Fung Chan,

Thanks a lot. It worked for me. Now i have an other issue. Currently i'm using Ubuntu on IMX53, how should i enable virtual keyboard at login and for typing.

0 项奖励
回复
4,515 次查看
jimmychan
NXP TechSupport
NXP TechSupport

I think you talk about the on-screen keyboard. I didn't try it on the i.MX board. but I think the following information may useful for you.

1. http://cmwelsh.com/enable-on-screen-keyboard-ubuntu-lucid-lynx

2. http://ubuntuforums.org/showthread.php?t=1392583

4,515 次查看
RandyKrakora
NXP Employee
NXP Employee

Did you see this yet?

https://community.freescale.com/message/228134#228134

Regards,

Randy

0 项奖励
回复
4,515 次查看
swaraj
Contributor II

Hi Randy,

     I have IMX53 Start-R board with the following information on the board:  SCH -27104 Rev B 700-27104 Rev X5. The link you have specified talks about the IMX53 QSB board.

Do we really need to do any modification on this version of Start-R boards to get the display. Please let us know.

Thanks,

Swaraj,

0 项奖励
回复
4,515 次查看
RandyKrakora
NXP Employee
NXP Employee

What are your uboot args?

Regards,

Randy Krakora

Field Applications Engineer

Freescale Semiconductor

(765)-860-6622

0 项奖励
回复