Hi,
I have installed mt9v022 camera module on the IMX-53 QSB-LOCO and after modprobe I have this:
Unable to handle kernel paging request at virtual address 4e454796
pgd = df720000
[4e454796] *pgd=00000000
Internal error: Oops: 5 [#1] PREEMPT
last sysfs file: /sys/devices/virtual/input/input3/capabilities/sw
Modules linked in: mt9v022(+)
CPU: 0 Not tainted (2.6.35.3-1129-g691c08a #25)
PC is at dev_get_drvdata+0x10/0x20
LR is at mt9v022_probe+0x12c/0x46c [mt9v022]
pc : [<8024000c>] lr : [<7f000fa0>] psr: 20000013
sp : df72fe70 ip : 0000ffff fp : 0000002e
r10: df702580 r9 : df72e000 r8 : 00000001
r7 : df144220 r6 : df702580 r5 : 80865fc8 r4 : df144200
r3 : 4e454756 r2 : 00000048 r1 : 00000001 r0 : 807b01a4
Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c5387d Table: cf720019 DAC: 00000015
Process insmod (pid: 2321, stack limit = 0xdf72e2e8)
Stack: (0xdf72fe70 to 0xdf730000)
fe60: df144200 7f0013d8 00000000 df144220
fe80: 7f0013d8 df144200 7f000e74 df144204 df72e000 00004000 00000000 802d222c
fea0: df144220 df144254 7f001838 7f001838 80034104 80240418 df144220 df144254
fec0: 7f001838 00000000 80034104 80240534 7f001838 df72fee0 802404d4 8023fc28
fee0: df031838 df082570 7f001838 7f001838 df6d6120 8088f560 00000000 8023f564
ff00: 7f0017ce 7f0017ce 00000000 7f001838 00000000 7f001810 8088f560 80034104
ff20: 00004000 80240824 8088f53c 00000000 7f001810 8088f560 80034104 802d2f68
ff40: 7f004000 00000000 00000000 00003a49 80034104 80033380 7f004000 00000000
ff60: 00000001 00000000 7f001970 00000000 00012008 80034104 df72e000 00004000
ff80: 00000000 8008e788 00012018 00003a49 00012008 00000002 7ee42ec9 00012018
ffa0: 00000080 80033f80 00000002 7ee42ec9 00012018 00003a49 00012008 0000002d
ffc0: 00000002 7ee42ec9 00012018 00000080 00000003 00000000 00004000 00000000
ffe0: 00012008 7ee42c5c 0000892c 2ab94fc4 60000010 00012018 76dfdabf 8db85ff6
[<8024000c>] (dev_get_drvdata+0x10/0x20) from [<7f000fa0>] (mt9v022_probe+0x12c/0x46c [mt9v022])
[<7f000fa0>] (mt9v022_probe+0x12c/0x46c [mt9v022]) from [<802d222c>] (i2c_device_probe+0xa4/0xd8)
[<802d222c>] (i2c_device_probe+0xa4/0xd8) from [<80240418>] (driver_probe_device+0xc8/0x184)
[<80240418>] (driver_probe_device+0xc8/0x184) from [<80240534>] (__driver_attach+0x60/0x84)
[<80240534>] (__driver_attach+0x60/0x84) from [<8023fc28>] (bus_for_each_dev+0x48/0x84)
[<8023fc28>] (bus_for_each_dev+0x48/0x84) from [<8023f564>] (bus_add_driver+0x98/0x214)
[<8023f564>] (bus_add_driver+0x98/0x214) from [<80240824>] (driver_register+0xac/0x13c)
[<80240824>] (driver_register+0xac/0x13c) from [<802d2f68>] (i2c_register_driver+0x40/0x8c)
[<802d2f68>] (i2c_register_driver+0x40/0x8c) from [<80033380>] (do_one_initcall+0x58/0x1b0)
[<80033380>] (do_one_initcall+0x58/0x1b0) from [<8008e788>] (sys_init_module+0x90/0x1ac)
[<8008e788>] (sys_init_module+0x90/0x1ac) from [<80033f80>] (ret_fast_syscall+0x0/0x30)
Code: e3500000 0a000003 e5903004 e3530000 (15930040)
---[ end trace 878551c919f71e5a ]---
Segmentation fault
Can someone help on this?
Thanks in advance