Seeking for Prcessor which do not need OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Seeking for Prcessor which do not need OS

1,309 Views
TEMCEFF
Contributor IV

Hello everyone... We Efftronics systems Pvt ltd are developer of various Embedded systems. Mostly we are using Cortex-M controllers for our applications.Now, we wanted to move to Cortex-A processors for our high end applications. As we have seen everywhere, processors are dealing with OS but we are seeking for processors which do not need OS means which can run without OS. Why we are asking like this is, when we go to OS like things, it mess up.. so we think to not use OS.

Please anyone suggest some solution...and what is the importance of OS in processors..?

Tags (1)
0 Kudos
Reply
4 Replies

1,101 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sathwik

one can look at i.MX6UL  FreeRTOS

Board Support Packages (7)
SDK2.2_iMX6UL_WIN(REV SDK2.2)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-processors/i.mx-6-pr...

i.MX 6UltraLite Applications Processor|NXP 

Operating systems (Software) facts, information, pictures | Encyclopedia.com articles about Operatin... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,101 Views
TEMCEFF
Contributor IV

Hello Igor...thanks for your reply.

i.Mx6, does this really don't need OS??  Can I program this processor with my regular C language coding skills??

Can I manage multiple cores without OS??

Finally, what I need is Processor which do not need OS for any reason?? Does this i.Mx6 series comply my need?

0 Kudos
Reply

1,101 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You may look at example in the following thread 

https://community.nxp.com/docs/DOC-103736 

Regards,

Yuri.

0 Kudos
Reply

1,101 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sathwik

one can also look at baremetal SDK:

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

>Can I manage multiple cores without OS??

yes. However it requires more programming skills and hardware knowledge,

compared with OS usage.

>Finally, what I need is Processor which do not need OS for any reason?? Does this i.Mx6 series comply my need?

i.Mx6 series can be used without OS, with baremetal codes. There is one exception case: graphics/video

(gpu/vpu modules in some processors) which can be used only with OS.

Best regards
igor

0 Kudos
Reply