Security Configuration in HAB4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Security Configuration in HAB4

ソリューションへジャンプ
3,594件の閲覧回数
jdepedro
Contributor IV

According to the CST-2.3.2 documentation, the "Security Configuration"  argument should not be present in the CSF description file when using HAB4. Yet the AN4581 (for HAB4) always uses "Security Configuration = Open" in all its CSF description file examples.

  • What exactly does that argument do?
  • Can it be safely removed when using HAB4?
ラベル(1)
タグ(1)
1 解決策
3,202件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   according to Table 3 (Header arguments) of the HAB Code-Signing Tool

User’s Guide, Security Configuration option relates to fused security configuration,

that may be as "Engineering" or "Production" and is used for HAB3.

   Please use the recent AN4581 (Rev. 1, 10/2015).

http://cache.nxp.com/files/32bit/doc/app_note/AN4581.pdf?fsrch=1&sr=1&pageNum=1

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
3,203件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   according to Table 3 (Header arguments) of the HAB Code-Signing Tool

User’s Guide, Security Configuration option relates to fused security configuration,

that may be as "Engineering" or "Production" and is used for HAB3.

   Please use the recent AN4581 (Rev. 1, 10/2015).

http://cache.nxp.com/files/32bit/doc/app_note/AN4581.pdf?fsrch=1&sr=1&pageNum=1

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

3,202件の閲覧回数
jdepedro
Contributor IV

Hi Yuri,

thanks for your answer. The argument "Security Configuration = Open" is present in the imx-test examples, not in the AN; my bad.

Anyways, after your answer I assume that it is indeed only used for HAB3, and has no effect on HAB4.

0 件の賞賛
返信
3,202件の閲覧回数
Yuri
NXP Employee
NXP Employee

Correct : "it is indeed only used for HAB3, and has no effect on HAB4".

Regards,

Yuri.

0 件の賞賛
返信