Securing Flash Partition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Securing Flash Partition

1,910 Views
MichaelBMiner
Contributor IV

Hello,

 

I am looking to use the Yocto project and CAAM to create a secure flash partition on my custom board. Note I cannot use the SNVS as the device will not always be powered, the design does not allow for a battery. 

In my yocto project I am going to create a new 8MB partition and call it securednand. As the device is to ship out the door there is an End of Line configuration step. Here we will run a script as root to do the following:

  1. Log in as root over a serial connection
  2. Run caam-keygen to create a key ie. caam_key
  3. Store caam_key to the securednand partition
  4. Use dm-crypt to encrypt securednand with a password file to be stored in /root (or another user protected folder)
  5. When the caam_key is needed, a service will be run to decrypt the securednand, read the caam_key and use it as needed. 

Is there anything else I need to be doing? Is this a moderately deceny security strategy?

Labels (1)
Tags (2)
2 Replies

1,892 Views
MichaelBMiner
Contributor IV

I am thinking of revising my plan. I am not familiar with security but I want to do the following. 

  1. Log in as root over a serial connection
  2. Run caam-keygen to create a key ie. caam_key
  3. Store caam_key to the securednand partition
  4. Use dm-crypt to encrypt securednand with a password file to be stored in /root/dm-crypt-pw
  5. Use the caam_key to encrypt the file /root/dm-crypt-pw

Now on boot I need to decrypt securednand using /root/dm-crypt-pw to get caam_key. This seems like a cyclic dependency. Not sure how to get around this. 

1,869 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please have the reference - the section <10.5 Disk encryption acceleration> of IMX_LINUX_USERS_GUIDE.pdf 

 

Regards

Harvey