Secure boot log imx7 if boot fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Secure boot log imx7 if boot fails

跳至解决方案
2,179 次查看
agalal
Contributor I

Hello Folks,

I am not a secure boot guru but after checking the boot security settings on Security Reference Manual for i.MX 7D. I found the following:

In case of boot mode set to closed; All detected errors are logged, and the boot flow is aborted with the control being passed to the serial downloader.

How can I gain access to these log files if the flow is aborted? There is no point of logging if we don't have access to these logs.

Thanks a lot

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,989 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abdallah

for security boot details one can refer to AN4581 Secure Boot 

http://www.nxp.com/docs/en/application-note/AN4581.pdf 

in particular on p.8 it states

"When built with this configuration [secure], U-Boot provides extra functions for HAB, one

of those being access to HAB status logs."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,989 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  You can create request / ticket to get more details about Secure boot (under NDA).

Support|NXP 

Regards,

Yuri.

0 项奖励
回复
1,990 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abdallah

for security boot details one can refer to AN4581 Secure Boot 

http://www.nxp.com/docs/en/application-note/AN4581.pdf 

in particular on p.8 it states

"When built with this configuration [secure], U-Boot provides extra functions for HAB, one

of those being access to HAB status logs."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------