Secure Boot iMXM Mini two boards, different behavior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure Boot iMXM Mini two boards, different behavior

Jump to solution
1,941 Views
jimtaylor-vertiv
Contributor III

I programmed the fuses for an iMX8M Mini board, loaded a signed image and watched it boot without HAB errors. After that I programmed the security bit so that the board would not boot without a valid image. The board continued to boot just fine.

I programmed the fuse on a second board the same way I programmed them on the first board. I loaded the same image and I am seeing HAB errors.

I then went into u-boot on both boards and used the "fuse read" command to read the value of the fuses in Banks 6 and 7. The fuses are identical. The fuses in Banks 1 3 and 2 2 are also identical. 

Does anyone have an idea of where I should start looking?

 

0 Kudos
Reply
1 Solution
1,879 Views
jimtaylor-vertiv
Contributor III

Thanks for responding. The issue was that the CSF.bin file was constructed differently and incorrectly. Once this was corrected, both cards booted as expected.

View solution in original post

0 Kudos
Reply
2 Replies
1,880 Views
jimtaylor-vertiv
Contributor III

Thanks for responding. The issue was that the CSF.bin file was constructed differently and incorrectly. Once this was corrected, both cards booted as expected.

0 Kudos
Reply
1,884 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @jimtaylor-vertiv,

The behavior you are describing is strange!

To debug more on the same, provide me with full logs, including the HAB error.

 

Thanks & Regards,
Dhruvit.

0 Kudos
Reply