Secure Boot iMXM Mini two boards, different behavior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure Boot iMXM Mini two boards, different behavior

ソリューションへジャンプ
2,044件の閲覧回数
jimtaylor-vertiv
Contributor III

I programmed the fuses for an iMX8M Mini board, loaded a signed image and watched it boot without HAB errors. After that I programmed the security bit so that the board would not boot without a valid image. The board continued to boot just fine.

I programmed the fuse on a second board the same way I programmed them on the first board. I loaded the same image and I am seeing HAB errors.

I then went into u-boot on both boards and used the "fuse read" command to read the value of the fuses in Banks 6 and 7. The fuses are identical. The fuses in Banks 1 3 and 2 2 are also identical. 

Does anyone have an idea of where I should start looking?

 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,982件の閲覧回数
jimtaylor-vertiv
Contributor III

Thanks for responding. The issue was that the CSF.bin file was constructed differently and incorrectly. Once this was corrected, both cards booted as expected.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,983件の閲覧回数
jimtaylor-vertiv
Contributor III

Thanks for responding. The issue was that the CSF.bin file was constructed differently and incorrectly. Once this was corrected, both cards booted as expected.

0 件の賞賛
返信
1,987件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @jimtaylor-vertiv,

The behavior you are describing is strange!

To debug more on the same, provide me with full logs, including the HAB error.

 

Thanks & Regards,
Dhruvit.

0 件の賞賛
返信