Hi all
Does someone have experience for connecting two LPDDR2 ?
My customer plan to connect two LPDDR2 with i.MX7.
When 2 GB of memory capacity is used, we plan to use 2 LPDDR2 x32 1GB RAM in parallel.
It is assumed to be used with switching by CS [1: 0].
Unfortunately, we can't find out a reference schematics.
Does someone have a reference schematic ?
If yes, please share it.
Ko-hey
已解决! 转到解答。
Hello,
As for one LPDDR device - really we have here single package, but several devices.
Control DRAM signals DRAM_DQMx, DRAM_SDQSx, address and data lines DRAM_ADDRESSx,
DRAM_SDBAx, DRAM_DATAx, clock DRAM_SDCLK0 are common for all DRAM devices.
DRAM_CS0, DRAM_SDCKE0, DRAM_ODT0 select and control one device (CS0),
DRAM_CS1, DRAM_SDCKE1, DRAM_ODT1 - the second.
Regards,
Yuri.
Hello,
You may look at WaRP7|NXP
The following about LPDDR3 and LPDDR2 differences may be useful:
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
As for one LPDDR device - really we have here single package, but several devices.
Control DRAM signals DRAM_DQMx, DRAM_SDQSx, address and data lines DRAM_ADDRESSx,
DRAM_SDBAx, DRAM_DATAx, clock DRAM_SDCLK0 are common for all DRAM devices.
DRAM_CS0, DRAM_SDCKE0, DRAM_ODT0 select and control one device (CS0),
DRAM_CS1, DRAM_SDCKE1, DRAM_ODT1 - the second.
Regards,
Yuri.