Sabresd stopped booting after adding .space value in file mx6_plugin.S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabresd stopped booting after adding .space value in file mx6_plugin.S

818 Views
mrigendra_chaub
Contributor III

Hi all,

I am not very good with assembly.

I have a i.mx6qp based board that is having checks for different skus in flash_header.S.

I want to port all these changes to the newer mx6_plugin.S file, but I am having difficulties in understanding some of the errors I am getting,

This is the file mx6_plugin.S

/*
* Copyright (C) 2016 Freescale Semiconductor, Inc.
*
* SPDX-License-Identifier: GPL-2.0+
*/

#include <config.h>

#ifdef CONFIG_ROM_UNIFIED_SECTIONS
#define ROM_API_TABLE_BASE_ADDR_LEGACY 0x180
#define ROM_VERSION_OFFSET 0x80
#else
#define ROM_API_TABLE_BASE_ADDR_LEGACY 0xC0
#define ROM_VERSION_OFFSET 0x48
#endif
#define ROM_API_TABLE_BASE_ADDR_MX6DQ_TO15 0xC4
#define ROM_API_TABLE_BASE_ADDR_MX6DL_TO12 0xC4
#define ROM_API_HWCNFG_SETUP_OFFSET 0x08
#define ROM_VERSION_TO10 0x10
#define ROM_VERSION_TO12 0x12
#define ROM_VERSION_TO15 0x15

plugin_start:

push {r0-r4, lr}

imx6_ddr_setting
imx6_clock_gating
imx6_qos_setting

/*
* The following is to fill in those arguments for this ROM function
* pu_irom_hwcnfg_setup(void **start, size_t *bytes, const void *boot_data)
* This function is used to copy data from the storage media into DDR.
* start - Initial (possibly partial) image load address on entry.
* Final image load address on exit.
* bytes - Initial (possibly partial) image size on entry.
* Final image size on exit.
* boot_data - Initial @ref ivt Boot Data load address.
*/
adr r0, boot_data2
adr r1, image_len2
adr r2, boot_data2

#ifdef CONFIG_NOR_BOOT
#ifdef CONFIG_MX6SX
ldr r3, =ROM_VERSION_OFFSET
ldr r4, [r3]
cmp r4, #ROM_VERSION_TO10
bgt before_calling_rom___pu_irom_hwcnfg_setup
ldr r3, =0x00900b00
ldr r4, =0x50000000
str r4, [r3, #0x5c]
#else
ldr r3, =0x00900800
ldr r4, =0x08000000
str r4, [r3, #0xc0]
#endif
#endif

/*
* check the _pu_irom_api_table for the address
*/
before_calling_rom___pu_irom_hwcnfg_setup:
ldr r3, =ROM_VERSION_OFFSET
ldr r4, [r3]
#if defined(CONFIG_MX6S) || defined(CONFIG_MX6DL)
ldr r3, =ROM_VERSION_TO12
cmp r4, r3
ldrge r3, =ROM_API_TABLE_BASE_ADDR_MX6DL_TO12
ldrlt r3, =ROM_API_TABLE_BASE_ADDR_LEGACY
#elif defined(CONFIG_MX6Q)
ldr r3, =ROM_VERSION_TO15
cmp r4, r3
ldrge r3, =ROM_API_TABLE_BASE_ADDR_MX6DQ_TO15
ldrlt r3, =ROM_API_TABLE_BASE_ADDR_LEGACY
#else
ldr r3, =ROM_API_TABLE_BASE_ADDR_LEGACY
#endif
ldr r4, [r3, #ROM_API_HWCNFG_SETUP_OFFSET]
blx r4
after_calling_rom___pu_irom_hwcnfg_setup:

/*
* ROM_API_HWCNFG_SETUP function enables MMU & Caches.
* Thus disable MMU & Caches.
*/

mrc p15, 0, r0, c1, c0, 0 /* read CP15 register 1 into r0*/
ands r0, r0, #0x1 /* check if MMU is enabled */
beq mmu_disable_notreq /* exit if MMU is already disabled */

/* Disable caches, MMU */
mrc p15, 0, r0, c1, c0, 0 /* read CP15 register 1 into r0 */
bic r0, r0, #(1 << 2) /* disable D Cache */
bic r0, r0, #0x1 /* clear bit 0 ; MMU off */

bic r0, r0, #(0x1 << 11) /* disable Z, branch prediction */
bic r0, r0, #(0x1 << 1) /* disable A, Strict alignment */
/* check enabled. */
mcr p15, 0, r0, c1, c0, 0 /* write CP15 register 1 */
mov r0, r0
mov r0, r0
mov r0, r0
mov r0, r0

mmu_disable_notreq:
NOP

/* To return to ROM from plugin, we need to fill in these argument.
* Here is what need to do:
* Need to construct the paramters for this function before return to ROM:
* plugin_download(void **start, size_t *bytes, UINT32 *ivt_offset)
*/
pop {r0-r4, lr}
push {r5}
ldr r5, boot_data2
str r5, [r0]
ldr r5, image_len2
str r5, [r1]
ldr r5, second_ivt_offset
str r5, [r2]
mov r0, #1
pop {r5}

/* return back to ROM code */
bx lr

/* make the following data right in the end of the output*/
.ltorg

#if (defined(CONFIG_NOR_BOOT) || defined(CONFIG_QSPI_BOOT))
#define FLASH_OFFSET 0x1000
#else
#define FLASH_OFFSET 0x400
#endif

/*
* second_ivt_offset is the offset from the "second_ivt_header" to
* "image_copy_start", which involves FLASH_OFFSET, plus the first
* ivt_header, the plugin code size itself recorded by "ivt2_header"
*/

second_ivt_offset: .long (ivt2_header + 0x2C + FLASH_OFFSET)

/*
* The following is the second IVT header plus the second boot data
*/
ivt2_header: .long 0x0
app2_code_jump_v: .long 0x0
reserv3: .long 0x0
dcd2_ptr: .long 0x0
boot_data2_ptr: .long 0x0
self_ptr2: .long 0x0
app_code_csf2: .long 0x0
reserv4: .long 0x0
boot_data2: .long 0x0
image_len2: .long 0x0
plugin2: .long 0x0

The older code saved some part of OCRAM to keep hwid results. Same way I added just this code above plugin start,

HWID_SAMPLE_DEBUG:
.space 16, 0x55    ----->>>>adding some locations to be used for sku verification

plugin_start:

...

using just above macro makes sabresd plugin booting stopped.

What this change is doing so that sabresd plugin image stopped working, its just saving 16 locations only? Where such changes should be kept?

Maybe it is changing the offest of overall code. how can I keep it correct?

If i can't use this method then is there any other way that I can save hwids in OCRAM?

Labels (1)
0 Kudos
Reply
1 Reply

680 Views
igorpadykov
NXP Employee
NXP Employee

Hi mrigendra

seems more proper way is to add changes after plugin_start:
push {r0-r4, lr}
<---

or make custom macro like "imx6_ddr_setting".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------