Reboot problem on IMX6q with kernel 4.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reboot problem on IMX6q with kernel 4.1

1,857件の閲覧回数
christiancharre
Contributor I

Hi all, I'm using kernel 4.1 from yocto krogoth on an IMX6q board.

When i ask for the reboot, the board is not rebooted. After invastigation it appears that restart function in the DT_MACHINE_START have been suppressed, so there is no more restart function.

Can anyone tell me how IMX6q boards can still be resetted ?

Why was this function suppressed in last kernel ?

Thanks by advance.

Regards.

Christian

ラベル(3)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,622件の閲覧回数
_andev_
Contributor II

Hi Christian!

Did you resolve this issue? I have the same problem with a 4.9.11 kernel. I've added the 'mxc_restart' method to the DT_MACHINE_START table but reboot is still not working... Did you get it working?

Thanks!

Jorge

0 件の賞賛
返信

1,622件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   please use NXP Linux.  Linux command  "reboot" works.
Also, You may apply "shutdown -r 0".

Summary Page :

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信