SabreSD ENET_REF_CLK AC coupling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SabreSD ENET_REF_CLK AC coupling

Jump to solution
1,804 Views
mahi
Contributor IV

Hi community,

is there another reason for AC coupling at the ENET_REF_CLK input in SabreSD-design than adjusting the voltage levels?

In my design I want to use 2.5V for all the Ethernet-related stuff (NVCC_ENET, NVCC_RGMII and VDDIO of the PHY) so connecting ENET_REF_CLK directly (only with a series resistor at the PHY's output) should be OK - or did I miss something?

Best regards,

Martin

Labels (4)
Tags (2)
0 Kudos
Reply
1 Solution
1,620 Views
igorpadykov
NXP Employee
NXP Employee

HI Martin

I agree with you: with the same voltage for all the Ethernet-related stuff

connecting ENET_REF_CLK directly is OK.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,621 Views
igorpadykov
NXP Employee
NXP Employee

HI Martin

I agree with you: with the same voltage for all the Ethernet-related stuff

connecting ENET_REF_CLK directly is OK.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply