SabreSD ENET_REF_CLK AC coupling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SabreSD ENET_REF_CLK AC coupling

ソリューションへジャンプ
1,764件の閲覧回数
mahi
Contributor IV

Hi community,

is there another reason for AC coupling at the ENET_REF_CLK input in SabreSD-design than adjusting the voltage levels?

In my design I want to use 2.5V for all the Ethernet-related stuff (NVCC_ENET, NVCC_RGMII and VDDIO of the PHY) so connecting ENET_REF_CLK directly (only with a series resistor at the PHY's output) should be OK - or did I miss something?

Best regards,

Martin

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 解決策
1,580件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Martin

I agree with you: with the same voltage for all the Ethernet-related stuff

connecting ENET_REF_CLK directly is OK.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,581件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Martin

I agree with you: with the same voltage for all the Ethernet-related stuff

connecting ENET_REF_CLK directly is OK.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信