Sabre for Smart Devices SATA 5V Power Connection Current Supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre for Smart Devices SATA 5V Power Connection Current Supply

Jump to solution
1,829 Views
atillametetured
Contributor V

Greetings,

SATA specification demands capability of 1.5 A current transfer on each parallel power pin. This totals up to a 4.5A current requirement at its height for the 5V supply. The step up converter used by the Sabre board for smart devices (MAX8815) should not be able to supply this demand. Plus the main supply to the board is coming from a 5V 5A adapter. How is it possible to confirm to the SATA specification when the PS to the connector can only supply 1A to a 4.5A demanding component? Am I mistaken or misinterpreting something? Please clarify this.

Thanks in advance,

Mete

Labels (2)
0 Kudos
Reply
1 Solution
1,754 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

I believe you are right, sabre design does not fully satisfy sata

power supply current capability, however this may be easily fixed using

more powerful supply.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,755 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

I believe you are right, sabre design does not fully satisfy sata

power supply current capability, however this may be easily fixed using

more powerful supply.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,754 Views
atillametetured
Contributor V

Okay Igor thank you.

Regards,

Mete

0 Kudos
Reply